If the receipt is from Purchasing, the cost used for these postings is the purchase order unit cost. If the receipt is from Production, the cost used depends on whether the job was automatically closed when posting the transaction. If it was automatically closed, the cost used is the actual unit cost from the job. If the job is left open, the system uses the planned cost of the job and makes an inventory adjustment when the job is closed.
| Cost Method | Receipt Cost Posted |
|---|---|
| Average | Weighted average calculation with the result posted back to the Unit Cost field. |
| LIFO or FIFO | The record is created in the Item LIFO file, recording the date, time, quantity, and cost of the receipt. |
| Specific | Cost tied directly to the location/lot to which the item was posted. If it was posted to a location/lot that already had a quantity and cost, the new cost is tied to the location and an Adjustment transaction is posted to the Inventory Ledger Distribution Journal. The cost is also posted to the Unit Cost field. |
| Standard | Standard unit cost is not changed. |
| Cost Method | Issue Cost Posted |
|---|---|
| Average | Uses the value in the (Standard) Unit Cost field in the Item Costs form. |
| LIFO | Starting with the newest Item LIFO record, the system processes these records until the entire quantity is issued, using the cost tied to each of the Item LIFO records it uses. |
| FIFO | Starting with the oldest Item LIFO record, the system processes these records until the entire quantity is issued, using the cost tied to each of the Item LIFO records it uses. |
| Specific | Uses the cost tied to the location/lot from which the item is issued. |
| Standard | Issues the item at Standard cost. |
About Changing an Item's Cost Method - Actual
About Changing an Item's Cost Method - Standard
About Posting - Average Cost Method