If you choose to track costs at the item/warehouse level, existing Lifo/Fifo stacks will be divided out proportionally based on Item Warehouse quantities. Each existing stack will be replaced by a new stack for each Item Warehouse which has quantities on hand. This will be illustrated through the following examples.
Warehouse MAIN contains 80 on-hand and warehouse DIST contains 20 on hand. This example uses one stack for the item, with five separate entries.
| Quantity | Acct | Cost |
|---|---|---|
| 20 | 1200 | $5.00 |
| 20 | 1200 | $7.00 |
| 20 | 1200 | $4.50 |
| 20 | 1300 | $6.50 |
| 20 | 1200 | $7.00 |
After processing, there are now two stacks.
Stack #1: DIST
|
Stack #2: MAIN
|
Since DIST had 20% of the inventory, the stack for DIST received 20% of each row. MAIN received the remainder which matches up to the 80% of the net on hand it contains. The total for the item still contains the same number of entries for each cost. Thus, there is no impact to the cost of inventory and no journal entries are required.
The program will process all warehouses except the default warehouse, saving that for last. During the processing of each warehouse, quantities will be rounded, resulting in whole quantities in each. Any remainders are placed into the default warehouse. See Dealing With Fractional Quantitiesfor information about fractional quantities.
FIFO Item Rounding
|
| Warehouse | Qty on Hand |
|---|---|
| MAIN | 70 |
| DIST | 30 |
| Quantity | Cost |
|---|---|
| 25 | $5.00 |
| 25 | $7.00 |
| 25 | $4.50 |
| 25 | $6.50 |
Rounding to whole numbers will result in the following distribution:
One stack for DIST
|
Another stack from MAIN
|
DIST gets 30% of each stack row since it contains 30% of the overall inventory. 30% of 25 is 7.5 which is rounded up to 8. The remainder (17) goes into main. In this example DIST hits its limit of 30 so the last row will only contain 6. This is due to rounding of the other rows. Remainders are placed in MAIN and everything is balanced.
FIFO is processed top to bottom and LIFO is processed bottom to top. In the above example, the 6 for DIST and 19 for MAIN would be first in the list and thus the first row consumed during an inventory issue.
As the above example illustrated, keeping track of the allocated quantity in a warehouse is important. This may dictate a second pass through the stack to re-allocate any leftover quantities.
| Warehouse | Qty on Hand |
|---|---|
| MAIN | 70 |
| DIST | 25 |
| DIS1 | 5 |
| Original StackQty |
Stack Cost | DIS1 Qty | DIST Qty | MAIN Qty |
|---|---|---|---|---|
| 7 | $5.00 | 0 | 2 | 5 |
| 1 | $7.00 | 0 | 0 | 1 |
| 10 | $5.50 | 1 | 3 | 6 |
| 72 | $6.00 | 4 | 18 | 50 |
| 3 | $5.00 | 0 | 1 | 2 |
| 2 | $7.50 | 0 | 1 | 1 |
| 5 | $7.00 | 0 | 0 | 5 |
The last row would typically get a quantity of 1 for the DIST warehouse, but that would exceed the total for DIST, so the remainder, 5 goes into MAIN.
Now consider a slightly different overall on hand:
| Warehouse | Qty on Hand |
|---|---|
| MAIN | 69 |
| DIST | 25 |
| DIS1 | 6 |
allocation of that last stack row is slightly different:
| Original Stack Qty |
Stack Cost | DIS1 Qty | DIST Qty | MAIN Qty |
|---|---|---|---|---|
| 7 | $5.00 | 0 | 2 | 5 |
| 1 | $7.00 | 0 | 0 | 1 |
| 10 | $5.50 | 1 | 3 | 6 |
| 72 | $6.00 | 4 | 18 | 50 |
| 3 | $5.00 | 0 | 1 | 2 |
| 2 | $7.50 | 0 | 1 | 1 |
| 5 | $7.00 | 1 | 0 | 4 |
DIST can not take a quantity of 1, and this time, MAIN can only take 4. In this scenario, the system will take a second pass through and find the first warehouse where on-hand has not been exceeded, adding as much as is available until everything is allocated or until that warehouse exceeds it's quantity on-hand. The process will continue until all remaining quantities from the original stack have been allocated.
If an unbalanced scenario occurs where the sum of the item warehouse quantities is less that the sum of the stack quantities, anything that remains will be placed in the default warehouse. This is probably a very unlikely scenario, but should be addressed in case it occurs. It is most important to make sure the stacks can add up to the same totals as before the process to avoid any reason to post journal adjustments. Again, cost should not change by turning this option on.
Some items are not stocked in whole amounts. Thus, a quantity of 3.35 could be valid. As discussed above in the rounding section, whole quantities are placed in the warehouses during processing. Then remainders are placed in the default warehouse.
| Warehouse | Qty on Hand |
|---|---|
| MAIN | 70 |
| DIST | 30.5 |
Initial Stack
|
Results of Rounding to the Whole Number
|
Initially, only whole numbers go into DIST and remainders are placed into MAIN. When processing the last value for $6.50, at first, only 6 are placed in DIST leaving 19 remaining. However, there's only room for 18.5 in MAIN, so an extra 0.5 is left over.
Thus, as discussed above in the section on multiple accounts, a second pass occurs on the stack and the remaining 0.5 goes into DIST. Thus, everything adds up correctly.
It is possible that we have to deal with negative quantities. If everything on hand is negative, the above examples will cover the situation (only the signs will be reversed). However, a couple of examples with a mixed scenario should be explained. A mix scenario will be defined as one with some warehouses negative and some positive.
Example Item Stack
|
Example Item Warehouse Amounts
|
Since the overall quantity for the item is positive, there will be no negative entries in the stack. The warehouse percent allocations are based on a net quantity on hand for the item of 20. The stack will break out into the following three stacks again based on a percentage:
| Warehouse | Qty on Hand | Cost |
|---|---|---|
| MAIN | 1 | $5.00 |
| 2 | $5.50 | |
| 0 | $5.00 | |
| DIST | 8 | $5.00 |
| 12 | $5.50 | |
| 4 | $5.00 | |
| DIS1 | -2 | %5.00 |
| -4 | $5.50 | |
| -1 | $5.00 |
All remainders go into MAIN, which in the case is negative. For example, consider the middle entry for $5.50. Originally this row contained 10. Two were allocated to DIS1, leaving 8. 12 were allocated to DIST, leaving -4. That remaining result goes into MAIN.