Material Planner Workbench Overview
The Material Planner Workbench offers you an alternative
method for generating supply orders that satisfy requirements without
needing to run MRP or APS. The system considers the demands and supplies
at all warehouses across the entire plan horizon and creates planned supply
orders to cover all instances where the on-hand inventory is below safety
stock. The system places the item replenishment data on the Material Planner
Workbench, where you can review it, make changes, and firm it into purchase
orders, purchase requisitions, jobs, production schedules, MPS orders,
and transfer orders.
Material Planner Workbench Generation form
The Material Planner Workbench Generation form generates
planning data that will be used to populate the Material Planner Workbench
form. You can generate data from one of the following sources: MRP or
APS plan output, item replenishment data (that is, a netting of all demands
and supplies at the warehouses), or cross-referenced orders. The system
uses the following three methods to generate the planned supply orders:
- MRP, APS, or MPS - The system
copies the MRP, APS, and MPS data directly from the output tables
that populate the Planning Detail form. This is similar to the Order
Action Report form except that KANBAN/JIT are excluded and MPS items
are included.
- Item Replenishment - The Inventory
Below Safety Stock logic is used to select items that need to
be replenished.
- Cross-Referenced Orders - The
system scans a range of customer orders, projects, jobs, and production
schedules that have a basic cross-reference type but do not yet have
a cross-reference number assigned to them. The system ignores reference
types of Stocked.
The following chart shows which fields on the Material
Planner Workbench Generation form correspond to each source:
| MRP, APS, or MPS |
Item replenishment data |
Cross-referenced orders |
| Use Planned Data |
Warehouse |
Order |
| |
Item |
Project |
| |
|
Transfer |
| |
|
Job |
NOTE: Configured
items are not included in the generation.
Material Planner Workbench form
Once you have run the generation, open the Material
Planner Workbench form to view the planned orders.
NOTE: Not all item
information is stored in the data file generated by the Material Planner
Generation form. When you open the Material Planner Workbench form, some
item information is pulled from the Items form. If an item's Configuration
Flag field was selected between the time when you generated your data
and the time when you opened the Material Planner Workbench form, the
orders associated with those items can no longer be firmed and will cause
the process to stop. Delete these workbench records to continue firming
orders.
When data populates the Material Planner Workbench
form, it is divided into six views based on two sets of criteria.
If you're using MRP, APS, and MPS data or item replenishment
data, the records are assigned to views according to the following rules:
- If the item's MPS Flag field is selected on the Items form, then
the record is placed on the MPS Order view.
- For item replenishment data, if the current warehouse is not the
default warehouse, the record is placed on the Transfer Order view.
- If the item's Source field is set to Purchased, the record is placed
on the Purchase Order view, even if you do not have purchasing authorization.
- If the item's Source field is set to Manufactured and the Prod
Type field is set to Job on the Items form, the record is placed on
the Job view.
- If the item's Source field is set to Manufactured and the Prod
Type field is set to Prod Sched on the Items form, the record is placed
on the Production Schedules view.
- If the item's Source field is set to Transferred on the Items form,
the record is placed on the Transfer Order view.
If you're using mass cross-referencing, the records
are assigned to views according to the following rules:
- If the cross-referenced item's MPS Flag field is selected on the
Items form, the record is placed on the MPS Order view.
- For order cross-references, the Reference field on the Customer
Order Lines form determines which view the data will be placed on.
If the setting is either Inventory or Project, this record is not
included on the workbench.
- For project cross-references, the Ref field on the Project Resources
form determines which view the data will be placed on. If the setting
is Inventory, this record is not included on the workbench.
- For transfer cross-references, the Ref Type field on the Transfer
Order Lines form determines which view the data will be placed on.
If the setting is Inventory, this record is not included on the workbench.
- For job cross-references, the Reference Type field on the Job Materials
form determines which view the data will be placed on. If the setting
is Inventory, this record is not included on the workbench.
A Summary form allows you to see the domestic currency
value of the data currently loaded on the Material Planner Workbench along
with the value of only the items that are selected to be processed.
Related Topics
Firming
Planned Orders Through the Material Planner Workbench
Generating
Data for the Material Planner Workbench