Documents generated by Infor PCM Configurator or Infor PCM Document Automation can be attached to records on certain SyteLine forms. Select the record and click the “Display Documents” toolbar icon to open the Documents form, where the Infor PCM documents related to the record are listed.
The Configure button and Actions > Configure menu option are displayed only if the system is set up as described in Setting Up a Configuration Interface for an Item or Job - Infor PCM.
The Configure button and Actions > Configure menu option launch the Infor PCM Configurator. If the Configurator generates content in the form of a document, information about that document can be passed back to SyteLine in either a MFG Detail Rule or a SyteLineDocument Integration Rule.
If the Infor PCM Configurator uses a MFG Detail rule to pass information about a generated document back to SyteLine, the document is stored in the SyteLine Attached Documents form and is attached to the appropriate form and record. The MFG Detail rule specifies the AttachTo type, which is used to attach the document to the appropriate form:
The MFG Detail rule must be defined in the Infor PCM Design Studio. For information about setting up MFG Detail rules, see the Infor SyteLine Integration Guide for Infor Product Configuration Management.
If the Infor PCM Configurator uses a SyteLineDocument integration rule to pass information about a generated document back to SyteLine, the document is stored in the SyteLine Attached Documents form and is attached to the form and record used to launch the Configurator.
Both the MFG Detail Rule and the SyteLineDocument Integration Rule have a DocumentName field. This Document Name is displayed in the list of documents that are accessible through the “Display documents for the current object” toolbar button on these forms, when the appropriate record is selected:
The SyteLineDocument integration rule must be defined in the Infor PCM Design Studio. For information about setting up SyteLineDocument integration rules, see the Infor SyteLine Integration Guide for Infor Product Configuration Management.
The Generate Document button and Actions > Generate Document menu option are displayed only if the system is set up as described in Setting Up the Infor PCM Document Automation Interface.
The Generate Document button and Actions > Generate Document option launch the Infor PCM Document Automation tool. If this tool generates content in the form of a document, it passes information about that document back to SyteLine in a SyteLineDocument integration rule. The document is stored in the SyteLine Attached Documents form, and is attached to the form and record used to launch Document Automation. These documents are accessible through the “Display documents for the current object” toolbar button on these forms, when the appropriate record is selected:
If a Default Rule Set was defined in the Inventory Parameters form, then when you select the menu option or click the button, you enter Infor PCM Document Automation tool. Otherwise, the Configuration Rule Sets form is displayed so you can select a rule set to generate the document.
Note: The Configuration Rule Sets form does not belong to a default authorization group, so the system administrator must assign individual users to the form or create a group.
For information about setting up rule sets in Infor PCM Document Automation, see the Infor PCM Document Automation Installation and Setup Guide.
Working with Document (File) Attachments
Setting Up the Infor PCM Document Automation Interface
Setting Up a Configuration Interface for an Item or Job - Infor PCM