Average Costing Setup
Follow these steps to implement Average costing in
the system:
- Select the Post to Journal check box on the General Parameters
form to have all transactions which affect inventory post to the G/L
Inventory Distribution Journal. Clear the check box to suppress posting
to the G/L those transactions which may affect inventory.
- Set the Cost Method field on the Items form - General tab
to Average for all items. (Ideally, you will set this field at the
time the items are added to the Items form).
- Set the Cost Type field on the Items form - General Tab
to Actual. The cost type defaults from the Cost Type field on the
General Parameters form when adding new items.
- Enter the initial cost of each item into the Unit Cost field on
the Item Costs form.
- You can maintain cost details for both unit cost and Current unit
cost entities. When the beginning inventory balance is entered through
the stock adjust transaction, the quantity entered is valued at the
cost entered. If an item has no beginning inventory balance, zero
may be left in the Unit Cost field for the system to update as the
item is received into stock.
- If you have instructed the system to post inventory transactions
to the G/L by selecting the Post to Journal check box on the General
Parameters form, you must also set up the G/L account numbers
which the system uses for this interface.
The following account numbers need to be entered into
the associated codes and parameters for costing purposes:
Product Codes - WIP Tab
Material
Labor
Fovhd
Vovhd
Outside
Product Codes - Misc Tab
Only one account is needed for:
Inventory Adjustment
Product Codes - Applied Overhead Tab
Only one account is needed for each of the following:
Matl Fovhd Applied
Matl Vovhd Applied
NOTE: The Matl Fovhd
Applied and the Matl Vovhd Applied accounts are required only when overhead
is based on job material issues.
Departments
Fixed Ovhd Applied Acct
Var Ovhd Applied Acct
Direct Labor Applied Acct
Work Centers - Costing Tab
Fix Mach Ovhd Applied Acct
Var Mach Ovhd Applied Acct
Distribution Accounts - Inventory Tab
Inventory
Inventory Labor
Inventory Fovhd
Inventory Vovhd
Inventory Outside
Distribution Accounts - Sales/COGS Tab
COGS Matl
COGS Labor
COGS Fovhd
COGS Vovhd
COGS Outside
Distribution Accounts - In-Transit Tab
In-Transit Material
In-Transit Labor
In-Transit Fovhd
In-Transit Vovhead
In-Transit Outside
Related Topics
Costing
Overview