Firming MPS Orders
This process describes how to convert MPS receipts
into jobs or production schedules. The system converts the MPS receipt
depending on the Production Type setting on the Items
form.
| Production Type |
Converts To |
| Job |
Job-Firm |
| Prod Sched |
Routes to Generate Production Schedules form and creates production
schedules |
| Kanban/Jit |
Prevents you from firming order |
NOTES:
- If a job is to be created, you enter the job number and the
quantity of the release, and the system creates the job header
automatically. However, you must copy or create the routing and
bill of material.
- If a production schedule is to be created, the system takes
you to the Generate Production Schedules form.
To use this feature, follow these steps:
- Make sure the correct item is displayed on the Master Production
Schedule form.
- Select the MPS receipt you want to firm.
- Select the Firm button.
- If the Firm MPS Order dialog appears, follow steps 4-5.
- If the Generate Production Schedules form appears, follow
steps 6-7.
- In the Firm MPS Order dialog, enter the appropriate data in the
following fields:
- Job Prefix - Enter a job
prefix or accept the default of the next new job number.
- Original Quantity Released
- Enter the quantity to be produced for this job.
- Due Date - Enter the due
date for this receipt.
The default values display from information on the MPS receipt you
are firming, but you can overwrite the default values as necessary.
- Select OK to firm the receipt.
- On the Generate Production Schedules form, select the Process
button to generate the production schedule.
- If no operations exist for the item, the message, "Copy will
be performed from Current Operation to Operation," displays.
Click OK. A success message displays the number of production
schedule releases the system generates.
NOTE: You can also
use the Material
Planner Workbench to firm MPS receipts.
Related Topics
Master
Production Schedule
Material
Planner Workbench