Interpreting the Exceptions Report

This topic describes the details of the Exceptions Report output in its Detail and Summary view.

Detail Report

Outstanding Requirements

The outstanding requirements are the sum of three components:

Outstanding Receipt

The outstanding receipt quantities are made up of purchase orders, purchase requisitions, firmed or released jobs, released production schedules, and transfers.

Original Quantity

The original quantity is the original suggested order quantity created by running the APS Planning or MRP Planning activity.

Parent Item Transaction

A parent item transaction is caused by a job, MPS order item, planned order or production schedule for the item's parent that has been exploded down to that item.

Reference

The reference identifies the source of the receipt or requirement that is due. The reference consists of three parts:

Part 1

The first part maintains a code that identifies the transaction type as a requirement or receipt.

Requirement Types:

Receipt types:

Part 2

The second part of the reference field is the CO number, job, and job suffix numbers, PO number, Production Schedule ID, purchase requisition number or transfer number.

Part 3

The third part of the reference field is the operation, if it is a job; or the line/release, if it is a CO or PO.

EXAMPLE: A Reference Code of CO 12 3-1 means that this item corresponds to customer order number 12, line/release 3-1. A Reference Code of PJOB 55-0001 10 means that this item corresponds to Job 55-0001, and Operation 10.

NOTE: You may also see the above reference with an X preceding it; for example, XPO. This situation indicates that it has been cross referenced. Other valid cross references are: XCO, XJOB, XPJOB, XPREQ and XTRNR.

Alternate Materials

NOTE: Alternate materials apply only to APS.

In the Detail view, this report displays any alternate materials used in the BOM. The word "Alternate" displays next to the material if the APS Planning activity used an alternate material on a planned order, and then you firmed that planned order into a job or production schedule item and copied the current routing/BOM. See the help topic for the Alternate check box that appears on the Planning Detail form for more information.

Summary Report

Outstanding requirements are the sum of three components:

The scheduled receipt quantities are made up of purchase orders, purchase requisitions, firmed or released jobs, released production schedules, and transfers.

The on-hand quantity is the total gross quantity on hand for the item at all locations (minus the non-nettable stock).

The planned orders quantity is the original suggested order quantity created by running the MRP Planning or APS Planning activity.


Related Topics

Exceptions Report