After performing a cycle count, you must post the results of the count. The procedures for both the count and the posting are included in Doing a Cycle Count.
When you run the Cycle Count Posting activity, the system posts and deletes records that have the count quantity within the Cycle Tolerance cutoff quantity and which are not exceptions.
The Cycle Count Posting activity processes the cycle record using the following process:
The Cycle Count Adjustment Journal reference INV CC-A; uses the following account numbers:
NOTE: If an account number is specified in the Product Codes Cycle Inventory Adj account field, the system uses that account instead.
If no other cycle count records exist for this item, the Cycle Triggered and Count in Process options are cleared.
When it encounters an exception condition, the Cycle Count Posting activity changes the status of a record from Counted to Exception. The activity then proceeds to the next cycle count record.
Exception conditions include:
If the activity encounters one of these conditions, the system changes the status from Counted to Exception and does not post the cycle record.
If the Cycle Count Record setting is changed to Exception because the current location's on-hand quantity is now different from the on-hand quantity when the count started or because the quantity counted exceeds the location on-hand quantity plus the Product Code General cycle tolerance, you can post the record using this activity. Make sure you change the Cycle Status field from Counted to Exception.
If the Cycle Count Record setting is changed to Exception for any other reason, you must correct the error condition in order to post the cycle count record. You can also delete the cycle count record from the cycle count.