Shipping a Transfer Order
There are three ways to ship a transfer order.
Manually Ship
	- Open the Transfer 
	 Order Ship form.
- Select a transfer order to ship.
- In Filter-in-Place mode, use the remaining header fields to filter 
	 the transfer order line items that will display in the grid.
- After you exit Filter-in-Place mode, select, in the grid, all line 
	 items that you want to ship.
- Edit the quantity shipped as needed.
- Ensure that the From Location field is correct.
- To add additional lines, click Add 
	 Lines to open the Add Transfer Ship Line modal form.
- Enter the specifications for the new line, then click Add 
	 to return to the Transfer 
	 Order Ship form.
- Click Ship to ship the selected 
	 transfer order line items.
Use the Transfer Order Ship Pick List
	- Open the Transfer 
	 Order Ship Pick List form.
- Enter the appropriate data in these fields: 
	
		- Starting and Ending Transfer 
		 Numbers - Enter the starting and ending transfer numbers of 
		 records to be processed.
- Post Material Issues - Select 
		 this field to to pick the inventory and post the journal transactions. 
		 However, serial and lot-tracked items are not posted.
- Post as of Date - Enter the 
		 date or accept the default of the current system date.
- Reprint Pick List Items - 
		 Select All Text to reprint all items that have a previous pick 
		 list date. Select None to not reprint all items that have a previous 
		 pick list date.
 
- Click Print to execute.
Use the Combined Transfer Order Ship/Receive
This procedure will create the journal entries for 
 both the shipped and received inventory.
	- Open the Combined 
	 Transfer Order Ship/Receive form.
- Select a transfer order.
- In Filter-in-Place mode, use the remaining header fields to filter 
	 the transfer order line items that will display in the grid.
- After you exit Filter-in-Place mode, select, in the grid, all line 
	 items that you want to ship or receive.
- Edit the quantity shipped or received as needed.
- Ensure that the From Location and To Location fields are correct.
- To add additional lines, click Add 
	 Lines to open the Add Transfer Ship Line modal form.
- Enter the specifications for the new line, then click Add 
	 to return to the Combined Transfer Order Ship/Receive 
	 form.
- Click Ship/Receive to ship or 
	 receive the selected transfer order line items.
Related Topics
Transfer Orders 
 Steps