To implement standard costing in the system, use the following procedure:
This selection indicates that all inventory reports and transaction posting to the G/L are to use the item's standard cost.
This field is also maintained on the Items form, the Cost Type field of which defaults from the Cost Type field of the lnventory Parameters form when adding new items.
For standard costing, the system uses the Cost Method field on the Items form only to determine what material cost to post to a job to which the item is issued.
Because the Standard Unit Cost field cannot be updated, the standard cost must be established in a different way.
The Roll Current Unit Cost to Standard Cost utility rolls the purchased current cost to the standard cost when you save the form.
The Roll Current Unit Cost to Standard Cost utility rolls the purchased current cost to the standard cost when you save the form.
WIP Material
WIP Labor
WIP Fixed Overhead
WIP Variable Overhead
WIP Outside Services
Efficiency Factor = WC efficiency/100
Setup Cost/Unit = (total setup hrs * OPERATIONS setup rate /lotsize) / efficiency factor
Run Cost/Unit = (per unit run hrs * OPERATIONS run rate / efficiency factor
Material Cost = QTY per parent * Std BOM Unit Cost / (1.00 - Scrap %)
Labor Fixed or Variable Overhead = OPERATIONS [Fix Var] OH Rate * [(Total Setup Hrs/Lot Size) + Run Hrs Per Piece]/Efficiency Factor
Material Fixed or Variable Overhead = MATERIALS [Fix Var] OH Rate * [(QTY Per Parent * Std BOM Unit Cost]/1.00-Scrap %
Machine Fixed or Variable Overhead = OPERATIONS [Fix Var] OH Rate [Run Hrs Per Piece]/Efficiency
Fixed Overhead = Labor Fixed Overhead + Material Fixed Overhead + Machine Fixed Overhead
Variable Overhead = Labor Variable Overhead + Material Variable Overhead + Machine Variable Overhead
Only one account is needed for each of the following:
Fixed Material Overhead Applied
Variable Material Overhead Applied
Fixed Labor Ovhd Usage
Variable Labor Overhead Usage
Fixed Material Overhead Usage
Variable Material Overhead Usage
Fixed Machine Overhead Usage
Variable Machine Overhead Usage
NOTE: The Fixed Material Overhead Applied and the Variable Material Overhead Applied accounts are required only when basing overhead on job material issues.
Cost Budget
Purchase Cost
Material Usage
Labor Rate
Labor Usage
Routing
Fixed Overhead Applied Account
Variable Overhead Applied Account
Direct Labor Applied Account
Fix Mach Ovhd Applied Account
Var Mach Ovh Applied Account
COGS Material
COGS Labor
COGS Fovhd
COGS Vovhd
COGS Outside Services
After the completion of these steps, you are ready to start processing manufacturing transactions.