Using the Resource Gantt Chart – Web Client
If you are running the Resource Gantt Chart on a Web client, follow 
 these steps to specify which resources you want to analyze, and to change 
 your display options.
Selecting Resources to Display
When you open this form, the Select Gantt Data dialog box is 
 displayed.
	- To display all resources, select All 
	 Resources. 
	To select a specific resource list to display, clear the All 
	 Resources check box to enable the Selection Name field. 
	 Select a resource list. To create a new list of resources that will be included in the Selection Name field: 
		- Click Selections to 
		 display the Resource Gantt Chart 
		 Selections form. 
- Click the New button in the tool bar.
- Specify a name for your new selection.
- In the Resources grid, click and select a resource to include 
		 in your list.  Specify a sequence number for it.
- To add more resources, click the New button in the tool bar. 
		 Use the Up and Down 
		 buttons to move the resources up and down in the list.
- When all the resources you want to display are added to the 
		 list, save your changes and close the form.
- In the Select Gantt Data 
		 form, select your new list in the Selection 
		 Name field.
 
- In the Alternative field, 
	 accept the default of zero to work with the production data, or select 
	 an alternative plan number. 
- In the Start Date and End Date fields, define the 
	 date range for which chart data is loaded. The planning or scheduling 
	 horizon dates are used as the defaults.
- Click OK to populate the 
	 Gantt Chart with the selected data.
To edit an existing list in the Select 
 Data dialog box, select the list, click Edit 
 and follow the steps above. To delete a list, select it and click Delete.
To change the list of displayed resources in the Resource 
 Gantt Chart at any time, click the Select 
 Data icon in the top left corner of the chart.
Changing Display Options
To change display options, click the Options icon in the 
 top left corner of the chart. You can change these options:
	- Secondary Selection: Use this 
	 option to indicate the type of logic used when you select a particular 
	 bar in the display. 
	
		- None (the default value) 
		 shows only the selected utilization bar in yellow.
- Same Operation shows all 
		 operations working on the same load. This option is useful if 
		 the operation is interrupted due to a shift change and the load 
		 is reallocated to another resource. All utilization bars for this 
		 operation/load are shown in yellow.
- Same Job shows all utilization 
		 bars for the same demand (job, production schedule, MPS order, 
		 planned order, etc.) in yellow.
 
- Bar Text: Use this option to 
	 change the text that is displayed on the utilization bars. By default, 
	 the job number displays on the bar. You can display the operation 
	 number, the item number, or no text.
To change the time scale of the chart, use the Zoom In and Zoom Out 
 icons in the top left corner of the chart.
Highlighting Bars in the Chart
You can use highlighting to color all chart bars that meet specified 
 criteria. For example, you can color red all bars associated with late 
 orders or color blue all bars for a large order quantity.
To apply an existing highlight to the chart, click the Edit Highlights 
 icon in the top left corner of the chart, and select the highlight name.
To create and apply a new highlight:
	- Click the Edit Highlights icon in the top left corner of the chart 
	 and select Edit. The Gantt Highlights form displays.
- Click the New button in the tool bar to add a highlight.
- Specify the highlight name.
- Click in the grid to add a criterion (rule) for applying color 
	 to a bar. A criterion consists of: sequence, type, comparison operator, 
	 value, and optional substring comparison settings. 
- Criteria are rules associated with a highlight on the Resource 
	 Gantt Chart. You can add multiple criteria to a highlight. Therefore, 
	 for the graphical bar to be colored according to the highlight, the 
	 resource must meet the highlight's various criteria. - Complete these fields (click each link for more information): 
- Select Must meet all criteria 
	 if all the listed criteria must be met in order for a bar to be highlighted 
	 in the chart. If this field is not selected, only one or more criteria 
	 in the list must be satisfied.
- Click the color box to display the standard color dialog box, where 
	 you can select a color. This color is used as the highlight color 
	 for a bar that meets the specified criteria.
- Use the Up and Down 
	 buttons to change the sequence of the criteria.
- Save your changes and close the form to return to the Resource 
	 Gantt Chart form.
- To apply your new highlight, select the name of your highlight 
	 from the Highlight right-click menu option.
Analyzing the Displayed Data
The Gantt chart display consists of one row for each resource named 
 in the selection. The display is organized as follows:
	- Green bars represent periods of utilization for the resource shown 
	 in the left column.
- Red bars represent down time (for example, off-shift periods or 
	 shift-exceptions).
- When you select a bar, the color changes to yellow.
- Blank areas of a row represent idle time for the resource.
NOTE: When the Gantt 
 chart displays load for infinite resources, the load bars might display 
 stacked on top of one another. As a result, some of them may not be visible.
Click on a resource utilization bar to view details about the operation 
 the resource is performing and the demand it is working on during the 
 time period. Click on a downtime bar to view details about the reason 
 for and duration of the downtime.
The picture below illustrates three resources, each working on a single 
 operation in a routing.

Manually Adjusting Gantt Chart Data
The Resource Gantt Chart - Scheduler form allows direct manipulation 
 of the bars shown in the Gantt chart. Available adjustments are:
	- Changes to the start and/or end of an operation
- Moving an operation to a different resource
- Freezing a job or operation.
When you move a bar in the chart, the Gantt 
 Edit Operation form is displayed. The "from" resource, 
 start date, and end date indicate the original information from the chart. 
 Specify new values for these fields:
	- To Resource is the resource 
	 where you want to move the operation.
- To Start Date is the new 
	 start date of the operation
- To End Date is the new 
	 end date of the operation.
Click OK to complete the edit 
 of the operation and return to the chart. The bar on the chart is updated.
Manual adjustments are available whether the schedule is created by 
 a normal Scheduler run or through the Use 
 Planning Output for Scheduling planning parameter. Once manual schedule 
 adjustments are made through the Gantt Chart, the results are reflected 
 in all Scheduling analysis forms and reports available to the user, including:
	- Resource/Resource Group Load Profile - Scheduler
- Resource/Resource Group Utilization - Scheduler
- Resource/Resource Group Schedule
- Resource/Resource Group Summary Report
Related Topics
Resources 
 Overview