Using the Resource Gantt Chart – Windows Client
If you are running the Resource Gantt Chart on a Windows client, follow 
 these steps to specify which resources you want to analyze, and to change 
 your display options.
Selecting Resources to Display
When you open this form, the Select Data dialog box is displayed.
	- To display all resources, select All 
	 Resources, or select a resource list to display. 
	To create a new list of resources: 
		- Click Add. A list of 
		 resources is displayed in the Add 
		 a Resource Selection dialog box. 
- Specify a name for your new list.
- To add a resource to your list, select it and click >. 
		 
- When all the resources you want to display are added to the 
		 list, click OK to return 
		 to the Select Data dialog 
		 box.
- Select your new list.
 
- In the Alternative field, 
	 accept the default selection of zero to work with the production data, 
	 or select an alternative plan number. 
- Define the Gantt chart horizon in the Start and End 
	 date fields.
- Click OK to populate the 
	 Gantt Chart with the selected data.
To edit an existing list in the Select 
 Data dialog box, select the list, click Edit 
 and follow the steps above. To delete a list, select it and click Delete.
To change the list of displayed resources in the Resource Gantt Chart 
 at any time, right-click anywhere in the chart and choose Select Data... 
 from the menu.
Changing Display Options
Right-click anywhere in the Gantt chart display to change display options. 
 You can change these options:
	- Secondary Selection: Use this 
	 option to indicate the type of logic used when you select a particular 
	 bar in the display. 
	
		- None (the default value) 
		 shows only the selected utilization bar in yellow.
- Same Operation shows all 
		 operations working on the same load. This option is useful if 
		 the operation is interrupted due to a shift change and the load 
		 is reallocated to another resource. All utilization bars for this 
		 operation/load are shown in yellow.
- Same Job shows all utilization 
		 bars for the same demand (job, production schedule, MPS order, 
		 planned order, etc.) in yellow.
 
- Bar Text: Use this option to 
	 change the text that is displayed on the utilization bars. By default, 
	 the job number displays on the bar. You can display the operation 
	 number, the item number, or no text.
	- Time Scale: The data is displayed 
	 in a one-hour granularity.
- Highlight: Display all utilization 
	 bars that meet specified criteria in a specific color. For example, 
	 you can color red all bars associated with late jobs or color blue 
	 all bars for a large job quantity. See the next section for more information.
Highlighting Bars in the Chart
You can use highlighting to color all chart bars that meet specified 
 criteria. For example, you can color red all bars associated with late 
 orders or color blue all bars for a large order quantity.
To apply an existing highlight:
	- Right-click anywhere in the Gantt chart and select Highlight. 
	 The Edit Highlights form displays.
- Select the highlight,then click OK.
To create and apply a new highlight:
	- Right-click anywhere in the Gantt chart and select Highlight. 
	 The Edit Highlights form displays.
- Click Add to open the Add a Highlight form.
- Specify the highlight name.
- Click the Add button. The Add a Criterion form displays.
- Enter a criterion (rule) for applying color to a bar. A criterion 
	 consists of: type, comparison operator, value, color, and optional 
	 substring comparison settings. 
	Criteria are rules associated with a highlight on the Resource Gantt 
	 Chart. You can add multiple criteria to a highlight. Therefore, for 
	 the graphical bar to be colored according to the highlight, the resource 
	 must meet the highlight's various criteria. Complete these fields (click each link for more information): 
- Click OK until you return 
	 to the Resource Gantt Chart 
	 form.
- To apply your new highlight, select the name of your highlight 
	 from the Highlight right-click menu option.
Comparison Substrings
For data items that are text strings, you can select the option to compare 
 a subset of the string. You can also specify the color to apply to bars 
 for which the comparison is true. If a highlight includes multiple criteria 
 and all criteria must be true for a bar to be colored, you define the 
 color in the Add Highlights dialog box.
For example, if bars associated with orders for more than 20 units are 
 to be colored blue, the rule would have the type Order Size, the 
 comparison operator ">", and the value 20.
Analyzing the Displayed Data
The Gantt chart display consists of one row for each resource named 
 in the selection. The display is organized as follows:
	- Green bars represent periods of utilization for the resource shown 
	 in the left column.
- Red bars represent down time (for example, off-shift periods or 
	 shift-exceptions).
- When you select a bar, the color changes to yellow.
- Blank areas of a row represent idle time for the resource.
NOTE: When the Gantt 
 chart displays load for infinite resources, the load bars might display 
 stacked on top of one another. As a result, some of them may not be visible.
Click on a resource utilization bar to view details about the operation 
 the resource is performing and the demand it is working on during the 
 time period. Click on a downtime bar to view details about the reason 
 for and duration of the downtime.
The picture below illustrates three resources, each working on a single 
 operation in a routing.

Manually Adjusting Gantt Chart Data
The Resource Gantt Chart - Scheduler form allows direct manipulation 
 of the bars shown in the Gantt chart. Available adjustments are:
	- Changes to the start and/or end of an operation
- Moving an operation to a different resource
- Freezing a job or operation.
Manual adjustments are available whether the schedule is created by 
 a normal Scheduler run or through the Use 
 Planning Output for Scheduling planning parameter. Once manual schedule 
 adjustments are made through the Gantt Chart, the results are reflected 
 in all Scheduling analysis forms and reports available to the user, including:
	- Resource/Resource Group Load Profile - Scheduler
- Resource/Resource Group Utilization - Scheduler
- Resource/Resource Group Schedule
- Resource/Resource Group Summary Report
For more information, see Manually 
 Adjusting the Resource Gantt Chart.
Related Topics
Manually Adjusting 
 the Resource Gantt Chart 
Resources Overview