Using Invoice Batch Detail
Use the Invoice
Batch Detail form to add, update, and delete Customer and A/R
posted records from an invoice batch. You can either open this form directly,
or you can click the Invoice Batch Detail
button on the Invoice
Batches form. Before using this form you must already have
created an invoice batch on the Invoice
Batches form, and you must have assigned an
Invoice Batch Cutoff Day to
a customer on the Customers
form.
Add a customer to the invoice batch
- On the Invoice Batch Detail
form, select the invoice batch in the Invoice Batch field for which
you wish to add a customer. The choices here are all invoices that
have not been placed on another invoice batch.
- Select a customer in the Customer
field. If no customers are displayed in the Customer
field, that means either that no customers have the same close date
that is assigned to the invoice batch or all of the customers that
do have that close date are already assigned to another batch.
- Save the record. Among the fields on this form are: Former Amount, Payments,
Carry
Over, Invoiced This Period,
Charges,
Taxes,
and Invoice
Amount.
Add an invoice for a customer
- After you add a customer, in the grid area of the
Invoice Batch Detail form, click the Invoice
field to specify an invoice. Add as many as you like, each one in
a different row.
- Save the record. This connection between the invoice batch and
the customer's transaction is seen in the
Invoice Batch field on the A/R
Posted Transactions Detail form.
Update or delete records
On the Invoice Batch Detail
form, only those records where the invoice batch has not been printed
can be updated or deleted. You can select and delete individual invoice
records in the grid or delete the invoice batch record from this form.
Related Topics
Generate
an Invoice Batch
Invoice
Batch Overview