EU Code

This field is applicable only if the selected country is a member of the European Union (EU).

To define the EU code for a country, in the EU Code column, enter the two-character EU code the system is to use for the country. This is the EU code used to populate the EU Code drop-down lists wherever they appear throughout the rest of the system.

NOTE: The fields in this column are accessible only if the Activate EU Reporting check box has been selected on the General Parameters form.