Select this check box on the General Parameters form to hide parent grid columns in linked forms. If this field is selected, then when users access a linked form from a parent form, the columns from the parent form are hidden on the linked form, leaving fewer columns to view. If this field is not selected, columns from the parent form also display on the linked form.
You can set this option for individual users on the Users form. If the option is not set at the user level, it defaults to the setting on the General Parameters form.