Select the box if the freight charge should be taxed. If the box is selected, then the system determines whether the freight tax code on the CO header is exempt or not. Freight tax amounts are saved for tax reporting.
If the box is cleared, then the system ignores the freight charge for tax purposes.
NOTE: This field is enabled only if the tax code is part of an area-based tax system and the Tax Code Type is set to Rate.