Select the box to tax miscellaneous charges. If the box is selected then the system determines whether the Miscellaneous Charges Tax Code on the Customer Order header is exempt. Miscellaneous charges tax amounts are saved for tax reporting.
Clear the box to ignore miscellaneous charges for tax purposes.
NOTE: This field is enabled (and should always be selected) if the tax code is part of an area-based tax system and the Tax Code Type is set to Rate.