Option
Choose how the selected information is to be used. On some forms, this field is disabled if the copy TO field is left blank.
- Delete All - Deletes the information specified. In the routing example, this option does not resequence the Operation Numbers.
- Insert Range - Inserts the information and resequences the operation numbers. For example, if you copy a routing with Operations 10, 20, 21, and 22 to a blank routing, the Insert option resequences the numbers to 10, 20, 30, and 40.
- Replace Range - Replaces existing information. In the routing example, this option does not resequence the Operation Numbers.