NOTE: If the domestic currency is not Part of Euro and the Euro currency itself does not have Rate is Divisor set to Yes, the Euro triangulation conversion method is unchanged.
Your domestic currency is the Deutsche mark (DEM) and you have received a 100,000,000 Won payment from a South Korean company. The system will convert the amount to Euros (EUR) and then to DEM.
The DEM currency is Part of Euro. The Rate is Divisor field for the Won-EUR currency is set to Yes and the Won currency is not Part of Euro.
The DEM-EUR rate is 1.9557989 DEM to 1 EUR. The Won-EUR rate is 942.89 Won to 1 EUR. Because the Rate is Divisor field is set to Yes, you enter the exchange rate in the Exchange Rate fields as the amount of EUR to one Won (in this case, 0.0010605).
The system calculates the conversion as follows:
Domestic amount = Foreign amount * Won-EUR * DEM-EUR
or,
DEM = 100,000,000 * 0.0010605 * 1.9557989
The resulting amount of DEM is 207,412.47.
Your domestic currency is the Deutsche mark (DEM) and you need to invoice a South Korean company for a 100,000 DEM product. The system will convert the amount to EUR and then to Won.
Assume the exchange rates from the above example still apply.
The system calculates the conversion as follows:
Foreign amount = Domestic amount / DEM-EUR / Won-EUR
or,
Won = 100,000 / 1.9557989 / 0.0010605
The resulting amount of Won is 48,213,108.11.