Calculator

Use the calculator to calculate amounts and enter the result into a field.

If you start the calculator by selecting Calculate from the right-click menu in an enabled numeric field, the field's value is copied into the calculator. You may then begin your calculations using the mouse or keyboard.

You can also launch the calculator from the Explorer.

The "tape" at the top of the calculator shows the progression of calculations. Use the scroll bar to see the calculations that have scrolled out of view.

NOTE: The calculator returns a value that matches the format required by the field. If required for an integer value, the calculator rounds the value.

For more information, see Using the Calculator with the Keyboard and Using the Calculator with the Mouse.


Related Topics

Using the Calculator with the Keyboard

Using the Calculator with the Mouse