Entering a Reason Code

You can add new reason codes on these forms:

To add new reason codes:

  1. Open the appropriate reason codes form from the list above.
  2. Click in the first empty row at the bottom of the list.
  3. In the Code field, enter a three-character code to represent the reason for the transaction.
  4. In the Description field, enter up to a 40-character description of the reason for the transaction.
  5. If the Inventory Adj account field appears (it appears only on Misc. Issue, Misc. Receipt, and Transfer Loss reason codes forms), select an Inventory Adjustment account number to associate with the reason code.
  6. Save the new reason codes and close the form.

Related Topics