Setting Up a Parametric Tax System
NOTE:This topic is
intended to help U.S. companies set up SyteLine
systems to properly handle sales tax. The system must be completely set
up before any transactions are entered. Once the system is initialized,
it will charge sales tax on customer orders and calculate sales tax on
purchase orders. The system will generate proper tax records for invoicing
taxable orders.
- On the General tab of the General
Parameters form, select the Capitalize State Abbreviations
field. The system then capitalizes the state abbreviation in addresses.
- On the Tax
Systemsform, SyteLine
presumes that the main tax system (Sales Tax) will be set up
with Tax Mode set to Area for U.S. companies. Most of
the parameters on this form should be left at their default value,
except the following:
- Enter Taxable in Tax Code Label field.
- Enter Federal ID in Tax ID Label field.
- Set up a default Customer/Vendor Tax Code with a Rate
tax type.
- On the Tax
Parameters form, set the field values according to your company's
specific reporting and functionality requirements. The usual field
values for U.S. companies are:
- Cash Rounding Factor: 0.00.
- Prompt for Tax Discount:
cleared
- Print Tax Codes on Invoice:
cleared
- Print Tax Footer on Invoice:
cleared
- Prompt for State Tax: selected
- Two Exchange Rates: cleared
- On the Tax
Codes form, at least one tax code with a Rate tax type
must already have been created in Step 2. In general, for tax codes
with a Rate tax type in the U.S., the Include Price
and Include Misc fields should be selected.
- Create another tax code to accommodate sales tax exempting, with
the following values:
- Tax System: 1
- Tax Code Type: Exemption
- Tax Code: N
- Description: Sales Tax Exempt
- Tax Rate: 0.00
- Assess on Return: cleared
The SyteLine
system is now ready for valid transactions to be entered. If the defaults
in theTax Systems form have been entered accurately, new customers
entered into the Customers form will have appropriate tax codes.
Therefore, when customer orders and purchase orders are entered, they
will use the proper defaults and have the correct sales tax applied.
Related Topics
Entering
Tax Code Information
Entering
Tax Code Information (GST/PST)
Setting
Up Tax Systems