G & A
G & A has three fields:
- G & A Cost - The G & A cost displays.
- G & A WIP Relieved - If Revenue Recognition is selected in the WIP Relief Method field, the G & A WIP Relieved field is updated when you run the Print/Post Project Revenue Milestones activity. If Manual or Shipment is selected in the WIP Relief Method field, the G & A WIP Relieved field is updated when you run the Print/Post Project WIP Relief activity.
- G & A Adjustment - Enter the adjustment amount. Click the Post button to open the Print/Post Project WIP Relief form.