Overhead
Other includes these fields:
- Overhead Cost: The
overhead cost displays.
- Overhead WIP Relieved:
If Revenue Recognition is selected in the WIP Relief Method field,
the Overhead WIP Relieved field is updated when you run the Print/Post
Project Revenue Milestones activity. If Manual or Shipment
is selected in the WIP Relief Method field, the Overhead WIP Relieved
field is updated when you run the Print/Post Project WIP Relief
activity.
- Overhead Adjustment:
Enter the adjustment amount. Click Post
to open the Print/Post
Project WIP Relief form.