To add materials to project tasks, use the Project Resources form.
The Actions menu includes the option, Go to Demand Detail Chart APS, which opens the Demand Detail Chart APS form. This option displays a graphical representation of how the system uses supplies, on-hand inventory, and resource capacity to satisfy the demand at each level of the bill of material.
The % Complete tab shows percent complete information for a project resource.
The information on the % Complete Details tab differs from the Percent Complete tab in that it is broken down by cost code AND monthly period, giving you even more detail than is on the Percent Complete tab.
The Shipping tab displays transactions processed against this project using the Project Resource Shipping form.
The fields in the EU VAT tab are used by the European Union (EU). If the Activate EU Reporting field on the General Parameters form is not selected, this tab (or some fields on this tab) are disabled.