Create a Project
Before creating a project, set up the following information:
NOTE: The following
steps cover only the basic requirements to create a record.
- On the Projects form, select Actions > New to
add a new project.
- Enter a project number in the Project field, or let the system
choose a number for you when you save the record.
- Enter the date when the project was entered into the system or
accept the default value of the system date.
- Select the project type in the Type field.
- On the Address tab, select a Customer and Ship To number.
- On the General tab, select the product code in the Product Code
field.
- On the General tab, enter a date range in the Start Date
and End Date fields.
- Select Actions > Save to save the project record.
Related Topics
Projects Overview