Create a Revenue Milestone

  1. Choose the project number on the Revenue Milestones form. Only projects with a WIP relief method of Revenue Recognition display in the drop-down.
  2. Enter the milestone number in the Milestone Number field.
  3. Enter a description in the (Description) field.
  4. Enter the planned complete date on the General tab. The planned complete date is the date you expect to print and post the milestone.
  5. Enter the planned cost amounts.
  6. Enter the planned revenue amount.
  7. Select the milestone cost calculation method on the Revenue Recog tab. This is a required field:
  8. Select the milestone revenue calculation method:
  9. Select the Requirements tab to add requirements for each milestone. It is not necessary to have a requirement for a milestone.
  10. If you are utilizing advance payments, use the Create Advance Payment Invoice and Advance Payment Deduction Amount fields to add advance payment information.
  11. Save your changes.

Related Topics

Projects Overview