Crediting Tax-Exempt Customers

If a customer notifies you that it received an invoice that included taxes, and the customer is tax-exempt, use these steps to correct the problem:

  1. In the Tax Interface Invoice Tax Credit form, select the customer order invoice for which you want to credit the tax amount.
  2. Information about the invoice is displayed. Verify that it describes the invoice you want.
  3. Click Check Invoice in AvaTax to look up the selected invoice in the AvaTax database. The system displays the amount of sales tax that was calculated for the invoice.  
  4. If AvaTax has determined that it can reverse the transaction, Can Credit Tax is selected, and the Process Tax Credit button is enabled. If Can Credit Tax is not selected, go into AvaTax and ensure that the customer is listed as tax-exempt. Then try again to process the invoice in this utility.
  5. Click Process Tax Credit to post the exemption through AvaTax.

After the exemption is processed, Tax Credited is selected to indicate that the invoice has already been credited through AvaTax.

Notes


Related Topics

Setting up an Avatax Tax Interface