This topic lists and describes the reports available in Shop-Trak along with a sample of the report. Shop-Trak reports include transactions from Shop-Trak Edit Transactions, Unposted Job Transactions, and Posted forms.
Report Name |
Report Description |
Report Sample |
| Edit List Report | Provides information about those transactions that still reside in the Shop-Trak Edit Transactions form. There are multiple range options available when generating this report including employee, transaction type, dates, job, shift, department, and indirect code. | Edit
List Report |
| Employee Status Report | Lists the jobs and transactions that employees are actively working on. This report can be run for a specified date and various ranges including employee, indirect code, and department. | Employee Status Report |
| Indirect Labor Codes Report | Lists all indirect codes with the option of printing the corresponding barcodes, or just the plain text. | Indirect Labor Codes
Report |
| Item Serial Number Labels Report | Use this report to print off a range of
serial numbers, or print off the serial numbers for a specified
range. It can also be run for a starting and ending range
of items. Only serial numbers that have a status of “In
Inventory” will print. This report will print the serial
numbers on preformatted 1 x
4 labels. These labels could then be used to complete the
Shop-Trak
Job Material Serial Numbers Report.
The completed report could be used as an aid when actually
performing the transactions in Infor SyteLine to create the one-to-one
link between a serialized component material to the serialized
parent item.
Use the Report Options form to define the printer the labels will print to. |
N/A |
| Job Material Serial Numbers Report | Use this report as a document to collect
the serial numbers of the serialized job components.
Select the job number range. Select the Print Barcode Format check box if you want barcodes to display on the report. The serial numbers can be entered in manually into the blank Unit S.N. box, or the Shop-Trak Item Serial Number Labels Report can be run to print the serial numbers on labels that can be manually placed onto the report. |
Job Material Serial
Numbers Report |
| Job Status Report | Indicates the current status of a specific
job. Transactions still in Shop-Trak are displayed with
a description of “Running,” Unposted Job Transactions are displayed
with a description of “Unposted.” Posted Job Transactions
do not indicate a description but are reported in totals by operation.
This report can be generated for Materials and Labor individually or Both Material and Labor. The detail includes a comparison of Planned hours versus Actual hours by operation and work center. |
Job Status Report |
| Kanban Replenishment Log | Displays information regarding replenishments that were generated by employees on the shop floor. Kanban Replenishments work in conjunction with the Shop-Trak Item Profile. | Kanban Replenishment
Log |
| Planned Absence Report | Can be generated by Employee range, Shift
and/or Department range, and with all absence detail or planned
absence only. Dates can also be specified.
This report displays employees that are absent from work. The employee is considered absent if they are not “punched in” or a pre-planned absence exists in the Human Resource module. The Activity Since Midnight column indicates if there has been any activity for the employee since midnight. "Yes" indicates that there is a transaction in the Employee Attendance form, Unposted Job Transaction form, Shop-Trak Edit Transaction form, or Project Transaction form that has a transaction date after midnight of the day the report is run for. "No" indicates that there is a record in the Employee Attendance form, but the employee has no other transactions since midnight of the day the report is run for. Blank indicates there are no actual transactions or employee attendance records since midnight for the day the report is run for. |
Planned Absence Report |
| Pre-Generation Report | Use this report to analyze employee payroll hours and dollars prior to generating payroll. The Use Shop-Trak Payroll Processing check box must be selected on the Payroll tab of the Shop-Trak Parameters form in order to generate this report. | Pre-Generation Report |
| Reason Codes Report | Lists reason codes by class, code, and description. | Reason Codes Report |
| RTE Transaction Report | Use this report to review transactions for those employees flagged as RTE in the Shop-Trak Employee Profile form. | RTE
Transaction Report |
| Rules List Report | Displays defined rules within Shop-Trak. These reports can be generated for machine or rate rules. | N/A |
| Team ID List Report | Displays a list of available teams along with the work center they are assigned to and the description of the team from the Team Master file. (Paul what file is this? Can't find a form named this) | Team ID List Report |
| Time & Attendance / Delinquency Report | Used for exception reporting relative
to employee's shift code start and end times and the early in/late
out grace periods. It includes transaction types, start and end
times, job and operation numbers, daily detail, totals and planned
absences recorded in Infor SyteLine.
This report can be generated by various ranges including date, employee, shift, department, and/or indirect code. It can be generated in detail or summary form. Detail mode displays exception messages. To accommodate the wide variety of reporting needs for employees that work remotely, this report can also be run just for RTE employees by selecting the RTE Employees Only check box. The exception messages shown are based off of the employee’s assigned shift start and end time. The exception message “Added Manually” is displayed when a transaction is manually added through the Unposted Job Transaction form, or the Shop-Trak Edit Transactions form. “Added Manually” means the transaction has no start or end times. This is an indication that the transaction did not come from the Shop-Trak Shop Floor, therefore it must have been added manually. |
Time & Attendance
/ Delinquency Report |
| Time Sheet Display Report | A complete listing of an employee’s transactions. Quantities can be viewed as well as job, operation, hours, dates, and times. | Time
Sheet Display Report |
| Time Sheet with Sign-Off Report | Displays a daily summary of transactions
for a selected employee, department, date range, or supervisor.
Running this report is very similar to running a Payroll Generation process. Therefore, it is very important to note that all transactions for the specified date range must be posted. The report displays the employee’s daily start time, up until a non-paid break/lunch, then the time after the break/lunch, until punchout for the day. If the employee did not take a non-paid break or lunch there will be one transaction showing the punchin time and the punchout time. The Worked Hours column shows the total of the actual time the employee worked. If the employee has records in the Employee Attendance form (Paula what is this form? Couldn't find it) for vacation, holiday, sick or other, those hours will also be displayed. The report will display data according to how the Shop-Trak Payroll Generation Tables form is set up. It is important to understand how the overtime rules are defined before running this report. If questions arise as to how the hours were calculated, refer to the Payroll Generation Tables for the shift/department that the employee is in to help answer questions. The report also has an area for the employee and the supervisor to sign-off on to approve the hours for the period. |
Time Sheet with Sign-Off
Report |
| Transaction Audit Trail Report | Used for diagnosing transaction processing
and changes or updates made to transactions after they have entered
the Shop-Trak
Edit Transaction form. The
report was originally created for Shop-Trak support analysts to
help resolve issues. It has since been made available on
the Shop-Trak
Reports menu as a tool for
customers also. The report may be run for add, update, delete,
or transfer activity.
Display Differences Only – Will only display the transactions that have changed from the time they entered the Shop-Trak Edit Transactions form to the time they were transferred to Infor SyteLine. Export to CSV - Use this option to export the records to Excel. The records can then be sorted and filtered to see only the data required. |
Transaction Audit Trail
Report |
| Transfer to SyteLine Report | Displays all transactions in the Edit Transactions form that did not transfer to SyteLine successfully due to certain conditions. | Transfer
to SyteLine Report |
| Work Center Status Report | Indicates the employees actively working in the work center, transaction and operation types the employee is logged in to, transaction start time, and time elapsed. This report can be generated by work center or department range. | Work
Center Status Report |
Running the Shop-Trak Transfer to SyteLine Report