Use the Biometric tab of the Shop-Trak Employee Profile form to set up an employee for fingerprint scanning.
Shop-Trak requires an M2SYS Biometric Device to perform the fingerprint registration process. Also, the biometric scanning software needs to be installed on the workstation performing the fingerprint registration. More information on the M2SYS biometric hardware and software can be found on the M2SYS Accelerated Biometrics Web site at www.m2sys.com.
To set up Biometrics for an employee:
Biometric Approver - Check this option to designate this employee as an Biometric Approver. An Approver can override another employee’s scan if for some reason the other employee is unable to scan in successfully.
NOTE: The Shop-Trak Biometric Scanning Log located under the Shop-Trak Utilities menu records all attempts to scan, and each override, including who performed the override. This is useful if questions arise as to which Approver is scanning employees in.
Perform Biometric Registration - Click this button to start the employee fingerprint registration. The M2SYS interface displays and allows the employee to scan their finger and create a registration file. This registration file will reside within the M2SYS database and is tied to the employee profile ID.
NOTE: It is important to make sure that the M2SYS registration file database is included in a regular backup routine. If the registration files are lost, each employee will need to re-register.
Once they are registered, employees will be prompted to scan their fingerprint when:
The employee will be allowed three attempts to scan in. If the third attempt fails, the employee will need to find an Approver (usually a Supervisor) that has authorization to scan them in. The Approver will enter the employee’s Shop-Trak ID and use their own fingerprint to log the employee in.
After the fingerprint registration file is found in the database and verified, employees will be allowed to proceed and log in to Shop-Trak Shop Floor. Shop-Trak will not require a fingerprint scan when starting and ending transactions once logged in, or when performing other activities such as WIP Moves or viewing the Visual Dispatch.
Shop-Trak Employee Profile Form
Viewing the Shop-Trak Biometric Scanning Log