Shop-Trak Editing Transactions
After being entered into Shop-Trak Shop Floor, the
Indirect, Setup, Run, Move, Direct, Project, Service Repair Order,
and Work Center Labor transactions are held in the Shop-Trak
Edit Transactions form.
NOTE: Open
Team, Multi-Job, and Punch In transactions are also held in the Shop-Trak
Edit Transactions form. An Open transaction is one that
does not yet have an end time. When these transaction types are
ended, they are converted into Run, Setup, Indirect, or Direct transactions
depending on how the employee chooses to end the transaction.
The Shop-Trak Edit Transactions form contains more detailed information
than what the employee sees in Shop-Trak Shop Floor. Supervisors
or clerical personnel use this form to correct transactions due to employee
errors. They also use this form to add transactions due to a power
outage or computer malfunction. Any transactions that do not transfer
successfully will remain in this form until the error condition is resolved.
IMPORTANT: To
prevent certain users from seeing the pay rates listed on this form, the
user should be assigned to the Shop-Trak
Hide Costs group on the SyteLine
Users form. The Pay Rate
field will then display a percentage instead of a dollar amount.
To edit transactions:
- Open the Shop-Trak Edit Transactions
form.
- Unfilter to view all records or filter for specific records.
- Select a transaction and click Lock
to edit the transaction. Locking the transaction will stop it from
being transferred to Infor
SyteLine and
prevent the employee from using Shop-Trak Shop Floor during the editing
process.
- Make any needed additions or changes.
- If employees forget to punch out of Shop-Trak Shop Floor, they
will receive a message the next time they punch in stating "You
had forgotten to Punchout." Once employees click OK, they
will be prompted to end the open transaction. The transaction
will then display on the Shop-Trak Edit Transactions form with the
Forgot to Punchout check
box selected. Typically the total Hours will be close to 24
hours when this occurs. To correct this situation:
- Adjust the transaction's Daily
End Time and clear the Forgot
to Punchout check box. The transaction is now ready
to transfer and post to Infor
SyteLine.
If the employee was scheduled for automatic breaks and lunches,
but left early and forgot to punch out, delete any unused breaks
or lunches.
- If employees forgot to end Multi-jobs
or Punchin transactions, the
transactions must be ended using Shop-Trak Shop Floor. Supervisors
cannot adjust Daily End Times
using the Shop-Trak Edit Transactions form for these types of transactions.
Additional data is needed to convert the transactions to valid
types such a Run, Setup, or Indirect.
NOTE: The Daily Start Time and
Daily End Time will display in hours or minutes according to the Reporting Time Units set on the
Transactions tab of the
Shop Floor Control Parameters form.
- Depending on the transaction type, there may be associated data
that you can edit on the Detail,
Quantities/Loc/Lot, Serial Numbers,
Co-products, and Service Repair Order tabs. The
Backflush Lots and Backflush Serials tabs are
read-only.
NOTE: The Transaction Type cannot be edited
or changed. To correct the Transaction Type, the original transaction
will need to be deleted and the correct Transaction Type will need to
be added.
- Save the data.
- Click Unlock. Transaction
validation occurs to ensure integrity of the employee's payroll hours.
If improper editing creates a gap or overlap of transactions
start/end times, a warning message displays.
- To view and unlock all employees that you have locked, click the
Manage My Locks tab. To
refresh the list of locked employees, click Refresh.
To unlock all locks put in place as a result of editing transactions, click Unlock My Lock.
- Close the form.
NOTE: You
can only unlock those employees that you have placed in a locked
status. There is an additional utility, Unlock
Locked Employees, that the Administrator can use to remove
locks put in place by all editors.
Related Topics
Shop-Trak Edit Transactions
Form
Shop-Trak Default
Groups
Shop-Trak Date Definitions
Shop-Trak Unlocking Employee
Records
Running the Shop-Trak
Transfer to SyteLine Report
Shop-Trak Transferring & Posting
Transactions Automatically
Shop-Trak Transferring & Posting
Transaction Manually
Shop-Trak
Backflushing of Lots & Serials Overview