Shop-Trak Using Group Configurations for Multi-Site Logins

Shop-Trak has the ability to add Group Configurations for Multi-Site customers.  It allows users to log in to their appropriate site’s Shop-Trak without having to always use custom Shop-Trak URLs.  It will also work with the One-Click client install.

Set Up Configurations and Group Configurations

Prerequisite:  An Administrator must have performed the Shop-Trak installation.
  1. Create Configurations in the Shop-Trak Configuration Manager found at Start > All Programs > Infor > Shop-Trak > LCConfigMenu.  Select the Shop-Trak Configuration Manager button.  Within the Actions box, add Configurations as needed.

  2. Select the Groups button and add Group Configurations for your sites.  Mark which Configurations are associated within each Group Configuration.  Multiple Configurations in a Group Configuration will provide users a drop-down list to choose their Configuration.
  3. Run the Shop-Trak Web Server Configuration Manager, also found on the Shop-Trak Configuration menu.
  4. Se tup the URL paths that users will need to get to the Shop-Trak application. See below for URL path information.
  5. Send the URL to the client for the appropriate Configuration and/or Group Configuration.
  6. Shop-Trak users install Shop-Trak from the URL.

URL Path Information

The URL can be found by right-clicking and choosing Properties on the menu item Shop-Trak found under Start > All Programs > Infor >.  The URL with the added Configuration and/or Group Configuration information will be:
 
http://servername/path to Shop-Trak app /LabrTrak.application?configgroup=group&configuration=configuration
 
It is not necessary to use both configuration and configgroup parameters.  One is sufficient.
 
Examples of URL paths:

http://SLServer\LabrTrak\LabrTrak.application?configuration=Lincoln

http://SLServer\LabrTrak\LabrTrak.application?configgroup=EAST

http://SLServer\LabrTrak\LabrTrak.application?configgroup=EAST&configuration=Baltimore

Other Information