Shop-Trak Setting Up the Item Profile for Kanban Replenishment
Kanban replenishment is a feature of Shop-Trak
that allows shop floor employees to create replenishment orders based
on an Item Profile. Use the Shop-Trak
Item Profile form to set up a profile for each item that can be
replenished by employees on the shop floor.
To set up an Item Profile:
- Open the Shop-Trak Item Profile
form.
- Specify this information:
- Item - This is a required
field. Select the item from the Item list. The corresponding
description displays in the Item Description field.
- Location - This is
a required field. Select the location from the Location
list. The corresponding warehouse displays in the adjacent
field.
- Inventory Source
- Displays where the item originated, either Purchased, Manufactured,
or Transferred.
NOTE:
Item, Location, and Inventory Source make up the index for the record.
Once a record is saved, these fields cannot be changed. The
only way to add another location for an item is to add another item and
warehouse for the other location. If you no longer want the item/location/warehouse
record you can delete it.
- Max Open
- Specify the maximum number of released orders (purchase, job,
and transfer orders) that can be maintained within Infor SyteLine.
Once this limit is reached, no further replenishments can
be generated from the shop floor until the orders are processed.
If the limit has been met and another replenishment order
is generated, a message displays. For example: "The
maximum number of Purchase Orders are already open."
- Replenishment Method - This is a required
field. Specify the replenishment method:
- Fixed - Allows
the user to define the desired bin quantity.
- MRP
- Uses system plans to determine bin quantity. You can
view the plans on the Planning
Detail form.
- SyteLean
- Uses system plans to determine bin quantity. SyteLean will adjust plan quantities created
through MRP, taking into account
history and forecasts.
- If the method is MRP or SyteLean, Shop-Trak looks at the
records on the Planning Detail
form when replenishing an item.
- If there are only future
PLN records for the item:
- The order is created for the first PLN.
- The order receives the date and quantity from the PLN.
- The PLN record is deleted
and the order record takes its place on the Planning
Detail form.
- If there are PLN records with a date of today or prior to
today:
- An order is created.
- The order receives the date from the oldest PLN.
- The order quantity is the sum of all PLN
records with dates of today and prior to today. In
addition, the quantity will include the quantity from
any PLNs looking out the days
supply from today.
- The PLN records are deleted
and one order record takes its place on the Planning Detail
form.
- Dates on a Job created
by a Shop-Trak Replenishment:
- The job date is today.
- The job end date is the date on the oldest PLN.
- The job start date is calculated using backwards scheduling
from the job end date.
- Planning Parameters
Planning Parameters that affect what is seen
on the Planning Detail form include:
- Transfers online.
- CO and Forecast online.
- Mfg and PO online.
If these parameters are checked, orders are
added on the Planning Detail form when needed. For example, you
will see a CO record added to the Planning Detail form, but a PLN record for the CO will not be added until MRP runs again. Therefore, if there is no other
PLN for an item, Shop-Trak will not replenish,
as it won’t see a PLN. MRP will run at
the scheduled time, or it can be run manually if required.
- Order Type
- This is a required field. Select the type of order to
be created during Kanban replenishment
(Purchase Order, Job Order, Transfer Order, PO Requisition, or
Production Schedule). Based on the Order
Type selected, additional fields display. If new orders
are desired for each Kanban replenishment,
then the Order field (just
below the Order Type field) should be left blank. For Purchase
Orders, where the Order Number is left blank, the PO will be a
Regular type. Order types:
- Purchase Order
- Created in Planned status. Vendor will be the rank
one vendor/item cross reference if available. If there
is none, lead time will come from the item maintenance.
- Regular Purchase Order
Number - New line added as long as the Purchase
Order is in Planned status.
- Blanket Purchase Order
Number - New release added as long as Purchase
Order is in Planned status.
- Prefix may be used on the Purchase Order. If
a Prefix is entered, a new Purchase Order is created using
the Prefix and the next sequential number. For
example: Prefix of "ab" wil
create PO ab0001, ab0002, etc.
- Job Order
- Created with routing/BOM copied,
status will be set to Released so that it is immediately visible
on the Shop-Trak Shop Floor Visual Dispatch.
- Job
Order - Optional.
If entered, a new suffix will be added to the job
number specified.
- Alternate Routing
- If you want to use
the routing of another item, enter an item number. Leaving
this field empty will create the job with the current
routing of the item.
- Transfer Order - Created
in Planned status. New line added as long as Transfer
Order is in Planned status. Specify these additional
fields: To Site,
To Warehouse, From
Site, From
Warehouse.
- PO Requisition
- Created in Planned status. Select a PO Requisition Number.
A new line is added as long as a PO Requisition is in
Planned status.
- Production Schedule
- New Production Schedule ID and Production Schedule Item
will be created with routing/BOM
copied in Released status.
- Production Schedule
ID - New Production Schedule Release will be created
and released.
- Bin Qty - Number of units required per replenishment.
Available with Fixed method only.
- Replenishment Qty
- Threshold for order creation. This field can be left blank,
resulting in a new order for each Kanban
replenishment processed.
- Accumulated Qty - Displays the sum of quantities for each
Kanban replenishment processed. Once
this equals the Replenishment
Qty, an order will be created
and the field will display any remaining quantity to be processed
yet.
- Email
and CC - Specify the e-mail
address of the person that should receive an e-mail notification
that a replenishment has been generated for this item.
- Save the data and close the form.
Related Topics
Shop-Trak Kanban Replenishment Log