Using the Inventory Manager Workbench

The Inventory Manager Workbench is designed for a manager to monitor inventory planning, general stockroom activities, transfer order management, order fulfillment, and physical inventory control.

By default, the Inventory Manager Workbench utilizes these critical numbers:

Buttons

Use these buttons to open other forms:

Critical Numbers

The standard Inventory Manager Workbench provides four system-level critical numbers. To better understand a critical number calculation, right-click on the gauge and select Setup to read the calculation definition on the Critical Numbers Setup form for the number in question.

To change the critical number that is displayed, right-click on the gauge and select Critical Number, then select a different number.

To alter the type of gauge, right-click on the one you want to change and select Display Type.

Options

Select from these options:

Items Grid

This grid drives the bottom half of the form. Use the standard toolset toolbar to manipulate the item data; Filter-in-Place functionality is supported.

The columns in the grid are standard item fields. To maintain the fields, right-click in the Item Number column and select Details. Use the online help of the Items form to learn more about each field.

NOTE: User extended tables (UETs) are supported within the item grid.

Inventory Issue YTD

This item-specific critical number sums the cost of the inventory that left inventory.

Inventory Receipts YTD

This item-specific critical number sums the cost of the inventory that came into inventory.

NOTE: Use the horizontal slider bar between the Items grid and the data details to adjust viewing. Move the slider down to increase the number of rows visible in the Items grid. After filtering the item data, review the results if all rows are presented on the screen without needing to scroll up and down. After you have selected the item against which you want to view detailed data, move the slider bar up to increase the space allotted to show more rows in the data detail view.

Additional Options

Select from these additional options on the form:


Related Topics

About Workbenches