In WinStudio, the level of editing permissions required to create an application. Objects edited under Vendor Developer editing permissions are saved as Vendor default versions.
Permissions are assigned on the Users form. Vendor developer editing permissions allow developers to use FormControl. Vendor developers can make any type of change to an existing form and can create and delete forms. Vendor developers see only the Vendor default versions of forms and do not see user or group versions. In the Explorer, only Vendor developers can modify folders in the Master Explorer. Vendor developers do not see public or user folders. A Vendor developer has the same capabilities as an end user to view and modify folders in My Folders.