WinStudio
Use this dialog box to view all the components on the current form and to edit certain types of properties. Each row in the list represents a component on the form. Each column displays a property for the component.
| Column/Property | Description/Comments |
Name |
Specifies the internal name of the component, which must be unique to the form |
Type |
Specifies what type of component it is |
Data Source |
Specifies the source of data to which the component is bound |
Container |
Specifies the container, if any, to which the component belongs |
Tab Order |
Specifies the tab order number of the component |
Event |
Specifies the event to be generated when the user interacts with the component in run time |
Pane |
(Multiview and query forms only) Indicates the pane in which the component is displayed Valid values include:
|
Error? |
Indicates whether an error was generated when the component was created OK indicates that no errors were generated. |
Component Class |
Specifies the component class on which the component is based, if any |
Enabled When |
Specifies the conditions under which this component is enabled, if any |
Visible When |
Specifies the conditions under which this component is visible, if any |
Required When |
Specifies the conditions under which this component is required, if any |
From Base Form |
Indicates whether the component takes its value and properties from a base form |
From Master Device |
Indicates whether the component is part of the master device type for the form |
These are the components that are available for editing on the form.
These components are disabled and unavailable for editing unless you "unlock" them.
You can also copy and paste data from the grid into a spreadsheet for further searching or sorting of the entire list of components on a form.
To edit properties of a component, select the row for the component you want and then click Edit.
WinStudio launches the Form Component Properties dialog box, which you can then use to edit the selected component's properties.
NOTE: When working with a form that has been created as an extension of another form, you can override the default setting that prevents you from changing the properties for a component belonging to the original (base) form. To do this, in the Form Component Properties dialog box, first reset the From Base Form property to False; and then you can modify the component's other properties.
About Creating New Forms by Extension