WinStudio
Use this dialog box to create, copy, edit, delete, enable or disable event handlers for the current form. You can also change the order in which event handlers execute and find strings in event handler specifications.
The content of the event handlers list depends on how you open the dialog box:
NOTE: In any of these cases, if you are opening this dialog box from an extended form:
The grid in this dialog box displays this information about each event handler:
| Column | Description/Comments |
Event |
Indicates the internal name of the event for which the handler is defined |
Seq |
Indicates the order in which the event handler executes This zero-based list number is significant only when an event has multiple event handlers. You can change this sequence using the Up and Down arrows at the bottom of the dialog box. |
Type |
Indicates what type of event handler is defined |
Disabled |
When selected, indicates that the event handler is not to be executed |
Response |
Indicates how WinStudio is to respond when the event handler executes This tyically consists of a set of parameters that define what the handler is to do |
This dialog box includes these action buttons:
| Button | Description/Comments |
Event filter |
To specify a single event for which you want to view the defined handlers, use this drop-down list. To view all event handlers, select [ALL]. |
OK |
To finish working in the dialog box and save your changes, click this button. |
New |
To create a new event handler, click this button. This button launches the Event Handler Properties dialog box, which allows you to define the new event handler. |
Copy |
To copy an event handler, select the handler to copy and click this button. This is useful when you want to base a new event handler on an existing handler with changes. This button launches the Event Handler Properties dialog box, populated with the attribute for the handler you are copying. |
Edit |
To edit an existing event handler, select the handler and click this button. This button launches the Event Handler Properties dialog box, populated with the attributes for the specified handler. |
Delete |
To delete an event handler, select the handler and click this button. |
Cancel |
To cancel any changes made and close the dialog box, click this button. |
Handlers |
To filter the list of event handlers for the event generated by a handler of the type, click this button. This is enabled only when the current handler is of the type Generate Event. |
Find |
To search the list of event handlers for a particular handler, click this button. You can search by keyword, method, parameter, or other specifications. |
Up and Down arrows |
To change the sequence order of event handlers, use these buttons. These buttons are enabled only if an event has multiple handlers. |
Help |
To view the help topic for this dialog box, click this button. |
About Generating Events from Components
Create, Copy, Edit or Delete Event Handlers
Event Handler Response Types (WinStudio)
Maximum Length of Parameters and Values
Understanding the WinStudio Event Model
About Creating New Forms by Extension