WinStudio
Use this dialog box to create, copy, edit, or delete variables.
Forms use variables to communicate between themselves, and to save environment information across form executions. Some variables are temporary, but persistent variables are loaded to and from disk. Variables can be global or associated with a particular form. You can use variables for many purposes, including binding them to components and controlling the initial action of a form.
To open this dialog box, perform one of these actions while in Design Mode:
This dialog box:
NOTE: If you are opening this dialog box from an extended form:
This dialog box includes these action buttons:
| Button | Description/Comments |
Done |
To finish working in the dialog box and save your changes, click this button. |
New |
To create a variable, click this button. This button launches the Variable Properties dialog box, which allows you to define the new variable. |
Copy |
To copy a variable, select the variable to copy and click this button. This is useful when you want to base a new variable on an existing variable, with changes. This button launches the Variable Properties dialog box, populated with the attribute for the variable you are copying. |
Edit |
To edit an existing variable, select the variable and click this button. This button launches the Variable Properties dialog box, populated with the attributes for the specified variable. |
Delete |
To delete a variable, select the variable and click this button. |
Help |
To view the help topic for this dialog box, click this button. |
Binding Components to Variables
Create, Copy, Edit, or Delete Variables
Maximum Length of Parameters and Values
About Creating New Forms by Extension