WinStudio
Use this dialog box to import images to the forms database. This makes it possible to transport the image file with the form and eliminates the need to call the image from an external location.
Beneath the image display, the customized scope is displayed.
| Field/Button/Option | Description/Comments |
Select Image Area |
Shows the image files that have been added. Select a file to import, export, or delete. |
Display Option |
Specifies one of these display options for the default display of the image: Fit, Fill, or Actual. For more information, see Image Display Property. |
Image Display Area |
Displays the currently selected image. |
Done |
Click to close the dialog box. |
New |
Click to begin a new entry, and to open the Open File dialog box to select the new entry. |
Import |
Click to import a replacement image and update the currently selected image using the Open File dialog box. |
Export |
Click to export the image using the Open File dialog box. |
Delete |
Click to remove the image. |
Help |
Click to open the online help for this dialog box. |