WinStudio
Use the New Data Maintenance Wizard to quickly and easily create forms with their required SQL tables, IDOs, and components.
This wizard can be especially helpful when you want to build a completely new form without having to create the infrastructure for it first.
To access this wizard, you must first be in Design Mode. To start the wizard then, from the Form menu, select Definition > New Data Maintenance.
The New Data Maintenance Wizard provides a range of options you can use to create your form:
| Field or Option | Required? | Notes |
Name |
Yes |
Specify the name to be assigned to the new form and IDO. Form names must be unique within an application. |
IDO Project |
Yes |
Specify from the drop-down list which IDO project the new form is to be part of |
Form Type |
Yes |
Specify from the drop-down list which type of form is to be created. Options include:
|
Device Type |
No |
Specify from the drop-down list which device type is to be the default device type for this form. |
Based on Database Table |
No |
When selected, this option indicates that the new database table and IDO are to be based on an existing database table. Specify which table with the drop-down list to the right of this check box. After you specify the table, use the Get Schema button to retrieve the scheme of the specified table and display it in the Table Schema grid. |
Create Form |
No |
When selected, this option indicates that the wizard is to create the form. When cleared, this option creates the SQL table and IDO, but not the form itself. In this case, you can create the form later, using the New Form Wizard. |
Create Scripts |
No |
When selected, this option causes the wizard to generate SQL scripts based on any User-Defined (Data) Types (UDTs) and the table being created. After they are generated, the scripts display in the next page of the wizard. |
Get Schema |
No |
Use this button to retrieve and display the schema of the database table specified in the Based on Database Table options. When you click this button, the wizard displays the entire table schema in the Table Schema grid. |
Save Template |
No |
Use this button to save the current wizard settings as a job template to an XML file. This allows you to reload the template later, should you need to, and can be a valuable aid to form development, in case you need to recreate a form. |
Open Template |
No |
Use this button to open a previously saved wizard job template (XML file) and load its values into the wizard. |
Table Schema grid |
Yes |
For information about how to use this grid, see Table Schema /Column Properties Grid, below. |
Add Row |
No |
Use this button to add a row to the Table Schema grid. This creates a new table column and all of its property attributes. |
Delete Row |
No |
Use this button to delete the selected row (property column) from the Table Schema grid. |
Delete All Rows |
No |
Use this button to dlete all rows from the Table Schema grid at once. |
Use the grid on this page to define the table columns that are to be created. For each column, you can also set the property attributes that it defines. These are the properties you can set using this grid:
| Property | Required? | Notes |
Name |
Yes |
Specifies the internal name to be assigned to the column. |
Data Type |
Yes |
Specifies the Mongoose system data type to be used for the property. If you specify this setting first, Mongoose automatically selects an appropriate data type for the SQL Data Type setting, which you can then override if you want. If you are not particularly concerned with Mongoose system data types, you can leave this field blank and instead select the desired SQL Data Type. |
SQL Data Type |
Yes |
Specifies the data type as used by SQL. You can use either an existing SQL base type here, or a User-defined Data Type (UDT). If you specify the name of a UDT (that is, a non-SQL base type), the wizard prompts you to create the UDT, if it does not already exist. You can then use the wizard to generate the scripts for SQL to use. |
Property Length |
No |
Specifies the maximum length that the value for this property value can have. For string types, this specifies the maximum number of characters allowed. For numeric types, this specifies the maximum total number of digits the field can display. NOTE: Not all data types recognize this attribute. |
Required |
No |
Indicates whether the property value is required or not. |
Label String ID |
No |
Specifies the string that is to be used for the form component caption. If you specify a string that does not already exist, the wizard prompts you to either create it as a translatable string or use it as a literal value. |
Primary Key |
No |
Indicates whether the property is to be a primary key. |
Property Class |
No |
Specifies the name of a property class to be used in defining the property attributes. |
Decimal Precision |
No |
Specifies how many digits are to display to the right of the decimal point. NOTE: This attribute is recognized only by numeric types that display decimal values. |
Default Value |
No |
Specifies a default IDO property value to be used when creating or copying records. For more information, see Default Values for Components. |
About the New Data Maintenance Wizard
Creating a Form with the New Data Maintenance Wizard