- In WinStudio, go into Design Mode.
- From the Form menu, select Definition > New.
- In the first page of the wizard, select the Create
new form option, and then click Next.
- In the next page, complete the following required fields:
- Optionally, specify a default Device
Type, a Query
Form, and any comments.
Comments are stored with the form definition and do not appear anywhere
on the actual form.
- Click Next.
- In the next page of the wizard (Select Properties), specify
the properties of the IDO that are to be used with components in the
new form.
For more information, see New
Form Wizard, Select Properties page.
- Click Next.
- In the next page of the wizard (Properties),
you can specify:
- The order in which the properties are listed
- The captions for properties/components
- What component class, if any, is to be applied to each property/component
For more information, see New
Form Wizard, Properties.
- Click Next.
- (Optional) To create a template from the new form, select the Save
Template option.
- Click Finish.
WinStudio then creates the form and opens a rough draft version in Design
Mode.