WinStudio

Edit Divisors Dialog Box

Use the Edit Divisors dialog box to specify the units and divisors by which the Y-axis scale is to be marked and displayed. For example, if the Y-axis data is to be displayed using millions of dollars, use the fields in this dialog box to set that up. You would select the option that uses 1000000 as the Divisor and sMillions as the String. When the form is opened and the graph is rendered, the data for the Y-axis is then automatically divided by 1000000 and the label "Millions" appears next to the Y-axis.

NOTE: Just because you select an option such as "Thousands," that does not force the system to use that divisor. If the smallest data value being presented is not divisible by 1000 without the displayed value being too small (for example, 20, which would display as ".02"), the system ignores this setting. If the smallest data value being presented is large enough that an even bigger value can be used instead (for example, 30000000, which is more easily and clearly divisible by one million), then the system uses the larger divisor instead, in this case 1000000.

This dialog box provides three standard divisors and units, but you can define your own. You can, for example, define the Y-axis data to render as minutes for raw data provided as the number of seconds. In this case, you would use 60 as the Divisor and sMinutes as the String.

NOTE: If the string you want is not already defined on the system, and you do not define it using the String Properties dialog box, whatever you use in the String field is treated as a literal value. So, for example, if you try to use sMinutes as the string but do not define it as a recognized string on the system, the graph actually displays "sMinutes".  


Related Topics

About Graph Components

Adding a Graph Component

Additional Graph Settings Dialog Box