WinStudio
Use this dialog box to set up and maintain button or edit components that users use to adjust a graph component.
Note: This topic applies to the graphing tool, which is supported for backward compatibility. We recommend that, if you want to add charts or gauges to a form, use the newer FusionCharts tool instead. For more information, see Adding Charts or Gauges to a Form.
| Previous Button | Applies to: Button components Label: Previous Scroll the graph to the preceding section. |
| Next Button | Applies to: Button components Label: Next Scroll the graph to the following section. |
| Redraw Button | Applies to: Button components Label: Redraw Redraw the graph using any new settings. |
| Properties Button | Applies to: Button components Label: Properties Adjust the color, style, or other display properties of the graph. |
| X Limit | Applies to: Edit components Enter the maximum number of points to include on the x-axis. |
| Graph component | Specify the name of the associated graph component. |
Add Button or Edit Components to Graph Components