WinStudio
Use this dialog box to specify settings for a DataView.
| Field | Description |
| Mode | Select the mode of the DataView:
|
These fields are only enabled for Predefined DataViews.
| Field | Description |
| DataView | Select the name of the DataView. |
| Layout | Optionally, select a saved DataView layout. |
| Filter | Optionally, select a filter for the DataView. |
These fields are only enabled for DataSearch.
| Field | Description |
| Search Expression | Specify an expression for the DataSearch. |
| Value Filter | Select the type of filter to use for the DataSearch. |
| Search Source | Select the source for the DataSearch. |
These fields are only enabled for Drilldowns.
| Field | Description |
| Critical Number | Specify a critical number for the drilldown. |
| Drilldown | Specify which drilldown to show. |
| As Of Date | Specify the date from which to run the drilldown. |
| Group | Specify a group for the drilldown. |
| Date Range | Specify a date range for the drilldown. |
| Input Parameters | Specify any additional parameters for the drilldown. |