About DataViews

With DataViews, you have the ability to view, parse, sort, group by, and filter data from the application within user-definable views and layouts. The DataView setup is similar to an Excel spreadsheet, displaying data in columns. As with form personalization, the DataView structure supports user, group, and site level layouts. If needed, you can export the DataView to a printer, XPS file, or Excel .xls file. Additionally, you can navigate to the related maintenance form by clicking Details on the right-click context menu.

Types of DataViews

These types of DataViews exist:

DataView Setup

Use these forms to set up a DataView:

You can create a repository of DataViews for specific users and groups. To create a new DataView, you must select a base IDO. All properties of the IDO selected are then listed to allow the user to choose the exact information that they want to include in the DataView. The ability to customize the display name of a property is supported.

Advanced functionality, such as IDO linking and sorting options, can be populated on the DataView IDO Setup form.

DataView Results

A DataView Generation button is available for all forms in the application. When you click the button, the data displayed on the current form, obeying applied filters, is sent to the DataView Results form. On this form, you can group, sort, and sum data to promote advanced data analysis. To generate a hardcopy of the data, you can save the results as an Excel or PDF file, or send them to a network printer.

Saved Layouts

Each time DataView results are presented, you can save a copy of the layout, which includes any personalizations you have made. This eliminates the redundant task of grouping and sorting the results. Depending on how user permissions are configured, some users can save their changes to the different scope levels: user, group, or site.

Right-Click Actions Menu

On some DataViews, you can right-click on a column and select various actions. For example, you can drill down into the form where data maintenance or transaction entry is performed. You can also drill down into another DataView, or run an executable program, using the Actions menu.

The actions that are available on any DataView column are determined on the DataView Actions form. For more information, see Setting Up the Right-Click Action Menu for DataViews.

Security

Provisions can be put in place to control which data elements are available to which users. You can do this two ways:

Multi-Row and Multi-Column Layouts

DataViews and DataSearch results can include multi-row (stacked) layouts.


Related Topics

About the Workbench Suite

Displaying a DataView

Setting Up DataViews

About DataView Layouts

Adding a DataView to a Form

Creating an Event to Call DataView Results

Setting Up a DataView Filter

Configuring Data Sources for DataSearch