WinStudio
IWSApplication interface
Takes a font descriptor string as input and returns the value as a Font data type.
A "font descriptor" is a string consisting of a list of fourteen comma-separated values. For more information, see "Settings" below.
Application.FontFromFontDescriptor( string )
Part |
Description |
| string | Required. Consists of fourteen comma-separated
values:
Size,0,0,0,Weight,Italic,Underline,Strikethrough,0,0,0,0,0,FontFamily For more information about these values, see "Settings" below. |
Setting |
Description |
| Size | A decimal value representing the point size. |
| Weight | Range from 0 (non-bold) to 700 (bold). |
| Italic | 0 = Normal text. 1 = Italicized text. |
| Underline | 0 = Text not
underlined. 1 = Text underlined. |
| Strikethrough | 0 = Normal text. 1 = Text struck through. |
| FontFamily | Name of the font (family) to be used. |
The return value is a Font data type matching the font descriptor string.
This method must be used in conjunction with another method that requires a Font data type as input. It allows you to construct the Font data type from a font descriptor string.
When using this method, you must include the following comment above the Imports section in any global or form script:
'//<Ref>System.Drawing.dll</Ref>
Dim FontDesc As String
Dim newFont As Font
FontDesc = Application.GetBaseFontDescriptor()
newFont = Application.FontFromFontDescriptor( FontDesc )
If not IDONull.IsNull(newFont) Then
newFont = new Font( newFont, FontStyle.Bold )
FontDesc = Application.FontDescriptorFromFont( newFont )
End If
ThisForm.Components("FormCollectionGrid").SetGridRowColFont( 3, 2, FontDesc, True )
SetGridRowColFontByColumnName Method