WinStudio
IWSFormComponent interface, grid objects
Assigns a font face and size to be used in a specified cell, and automatically adjusts the height of the row, if necessary, to accommodate the assigned font.
object.SetGridRowColFont( integer1, integer2, string, Boolean )
Part |
Description |
object | Required. A reference to a grid component. |
integer1 | Required. Indicates the row number.
Row numbering is 1-based. |
integer2 | Required. Indicates the column number.
Column numbering is 1-based. If you use 0 (zero) for this value, the colors are applied to the entire row. |
string | Required. Font descriptor string consisting of
fourteen comma-separated values:
Size,0,0,0,Weight,Italic,Underline,Strikethrough,0,0,0,0,0,FontFamily For more information about these values, see "Settings" below. |
Boolean | Required. Determines whether the system should
adjust the height of the row, if necessary, to accommodate the
font face and size being assigned.
Unless you have specific reasons for doing otherwise, you should use a value of TRUE. |
Setting |
Description |
Size | A decimal value representing the point size. |
Weight | Range from 0 (non-bold) to 700 (bold). |
Italic | 0 = Normal text. 1 = Italicized text. |
Underline | 0 = Text not
underlined. 1 = Text underlined. |
Strikethrough | 0 = Normal text. 1 = Text struck through. |
FontFamily | Name of the font to be used. |
Sub Main() 'Sets the font for the specified cell to 12-point bold Times New Roman. Dim fontDescriptor As String = "12,0,0,0,700,0,0,0,0,0,0,0,0,Times New Roman" ThisForm.Components("grid").SetGridRowColFont(3, 1, fontDescriptor, True) End Sub
SetGridRowColFontByColumnName Method
SetGridRowColColorByColumnName Method
SetGridRowColImageByColumnName Method