\/b>
WinStudio
IWSIDOProperty interface
Retrieves a binary large object (BLOB), such as a graphic image, from a file and loads it in a specified item of a collection.
object.ImportBlob( string )
Part |
Description |
| object | Required. An expression that evaluates to the name of an IDO collection object (item). |
| string | Required. The name of an operating system file containing the BLOB. This string must include the path. The path can be relative to the directory containing WinStudio.exe. |
Deprecated. Now available only with item objects. Instead of this method, you should generally try to use the ImportCurrentObjectPropertyAsBlob or ImportObjectPropertyAsBlob method.
Sub Main()
Dim FileName As String
FileName = "C:\Temp\Splash_VBA_TEST.BMP"
ThisForm.PrimaryIDOCollection.CurrentItem.Properties("myItem").ImportBlob(FileName)
End Sub