The credit card processing system has three levels of reporting, which are used to determine if a certain transaction is a qualified transaction:
The specific data collected is unique to each credit card gateway and credit card type.
Select Level Three Reporting on the Credit Card Interface Parameters form if you want the credit card interface to send additional information in order to qualify for Level 3 processing. Otherwise, data qualified for Level 2 processing is collected and sent to the credit card system.
Line Tax: This application does not store tax amount detail at the invoice line item level. In order to send line level tax information (for Level 3 reporting) the effective tax rate for the whole invoice based on the tax amount is calculated and then spread over each individual line. This can result in an individual line showing as taxed even though it was exempt.
Customer Purchase Order: The Intrix API does not separate Customer PO and Customer Reference Code. This interface uses the Customer Reference Code as the PO in Intrix Level 2 data; the actual customer PO is not used.
Setting Up the Credit Card Interface