Setting Up the Credit Card Interface

Prerequisites

Use the Credit Card Interface Implementation Guide to install and implement the Credit Card Interface. During this process you must have this information:

This information is recorded on the Credit Card Interface Parameters form during the implementation.

NOTE: A test URL and test credit card numbers are provided in the Credit Card Interface Implementation Guide.

Credit Card Parameters form

On this form, specify this information:

  1. To connect to the third-party system:

    Credit Card System

    Specify the provider to which the credit card transactions are sent. Select External if you have developed an interface to a gateway that is not currently supported by the standard application.

    Caution: See "If You Switch Credit Card Systems," below.

    User ID and Password

    Specify the user ID and password provided by the third-party system to access their credit card processing software.

    Payment Server

    Specify the URL of the Web Service used for credit card processing. See the Credit Card Interface Implementation Guide for the appropriate URL.

    RP Number

    This field is displayed only if the Credit Card System is Hypercom. Specify the Merchant Number supplied by Hypercom.

    Vendor ID

    This field is displayed only if the Credit Card System is Intrix. Specify the Vendor ID supplied by Intrix.

    Merchant ID

    This field is displayed only if the Credit Card System is CenPOS. Specify the Merchant ID supplied by CenPOS. Then click the Configure SQL Connection link to display the CCIWebSetup.aspx page, where you specify the SQL user and password that the Web service will use to access the application database. This information is stored encrypted on the SyteLine Web server.

  2. Provide general information about how the interface is used:

Credit Card Payments form

For each of your customers who will pay by credit card, you can set up credit card information on the Credit Card Payments form and click Store for Future Orders to save the information.  (You can also fill out this form during entry of an order for the customer.)

Shipping Information

Set up Ship Methods to use on items shipped to credit card customers. See Setting Up Shipping Charges for Credit Card Customers.

Debugging the Interface

If it becomes necessary to track problems in your credit card interface, select Debug on the Credit Card Interface Parameters form and specify a folder to create a text file on the database server that lists the process steps that occur the next time you process a credit card through the interface. The file does not include sensitive information from the card.

If You Switch Credit Card Systems

If you change from one gateway provider to another, any pre-existing credit card transactions and any stored credit card information becomes invalid.

Use the Customer Credit Cards form to determine which customer credit cards were stored using the old system. These records must be deleted and re-entered using the new system and the Credit Card Payments form.

Use the Credit Card Transactions form to determine which transactions were in process and must be reauthorized using the new system.


Related Topics

About the Credit Card Interface

Using the External Option to Create Links to Other Gateways

Pre-authorizing Credit Card Amounts or Percentages

Troubleshooting Intrix Error Messages